SKIN PROTECTION AND FIRST AID
| Optimal skin protection in four stages. |
// General
Skin protection: an important preventative measure in the workplace
The skin is the largest organ of the human body. It has an important protective function and supports humans in immune defence. In occupational environments, the skin is constantly exposed to numerous harmful influences. This increases the risk of skin conditions.
38% of all occupational illnesses are skin diseases, as the skin is exposed to many harmful influences in the work environment. One of the most common skin diseases is dermatitis, which is caused by allergenic materials, chemical, or even poisonous substances.
The costs incurred from lost working days are correspondingly high; likewise, healing from skin conditions often takes a long time. For these reasons, skin protection at the workplace is of great importance in order to maintain the healthy condition of the skin.
-
Comprehensive skin protection protects against injuries or skin damage caused by:
- Working in a damp environment
- Contact with hazardous substances (such as chemicals, etc.)
- Physical effects (such as sharp edges or falling objects)
- UV radiation (such as burns)
- Working in a damp environment
- Working in a damp environment
- Contact with hazardous substances (such as chemicals, etc.)
- Physical effects (such as sharp edges or falling objects)
- UV radiation (such as burns)
When skin is appropriately protected in combination with regular hand hygiene, absences due to illness and high costs for treatment can be reduced by up to 40%.
// SELECTION AID
What to take into consideration when selecting products
So that your employees are optimally protected, skin protection starts even before work and is re-applied during work; these are preventative measures.
Skin protection prevents work materials from penetrating into the skin and serves as a protective barrier against harmful substances. This makes it easier to clean the skin.
Different skin protection products protect against things such as the following:
- Extreme dirt
- Strongly adhesive materials
- Water-based materials or wet work
- UV exposure
- Build-up of moisture
// SELECTION AID
Skin protection
Skin Care
Skin Care

Skin cleansing
Skin protection
Skin Care

Hand disinfection
Skin cleansing
Skin protection

Accessories
Hand disinfection
Skin cleansing

Accessories
Accessories
Hand disinfection

// SERVICES – Skin protection
Company skin protection plan – The perfect skin protection at work
Setting up a skin protection plan that matches your business proceeds through the following steps:
- The actual strains on the skin are identified by means of an on-site risk assessment
- Risk assessments are conducted by safety professionals and medical officers.
- The hazards at the workplace are documented in a skin protection plan, which also highlights suitable skin protection measures
The benefits of a specifically tailored skin protection plan at a glance
- Skin protection matching the actual working environments in your company.
- Greater likelihood that skin protection products are used properly.
- Products in the various departments used properly and at the right time.
- Take specific steps to avoid or prevent your employees from suffering skin diseases.
- Reduce costs caused by occupational diseases:
- Cut business costs.
- Improve productivity through better protection.
- Reduce employee absences.

// SERVICES – Skin protection
Company skin protection plan – The perfect skin protection at work
We’ll help you set up a skin protection plan for your business
A skin protection plan details the risks your skin faces during each job performed at your workplace. The plan ensures that your workforce will all use the skin protection products the way they’re meant to. The skin protection plan also lists the skin protection, skin cleansing and skin care products to use in order to keep your skin protected properly.
Why is a tailored skin protection plan necessary?
Many companies use model skin protection plans that fail to account for all risks to the skin posed at the respective workplace, and which assume that the employees’ skin is healthy to start with. A tailored skin protection plan will accommodate the requirements specific to every employee and also detail skin protection measures and skin care appropriate to the workstation.

Optimal skin protection in four stages.
We’ll take you through the four steps of setting up your ideal skin protection plan – to create transparent skin safety for the best-possible protection of your workforce. Get the complete package of competent advice, skin protection plan drafting and comprehensive product range to gain perfect skin protection before, at and after work that will keep your skin well and healthy.
// SERVICES – Skin protection
Drafting a skin protection plan
We’ll set up a skin protection plan for you based on what we’ve learnt from our consultation and the tour of your premises and provide you with the draft.
// SERVICES – Skin protection
Consultation
Our qualified PPE specialist is on call to meet at your premises for a tour of your workplace and to make a record of the jobs handled at your various workstations. We’ll use these records to draw up a selection of suitable skin protection products for you to choose from and then assist you in sampling and testing them.
// SERVICES – Skin protection
Ordering
Once we’ve completed the tour of your workplace and any tests have been passed, you can place your first order with us. Just let us know what products you want to use where and what jobs you need them for.
// SERVICES – Skin protection
Sending the skin protection plan
Are you happy with your skin protection plan? Then we’ll send you your tailor-made skin protection plan.
// FIRST AID
First aid in the workplace
Despite all precautionary and protective measures, employees may be injured while at work. In order to be able to help them quickly, first aid in the workplace is of utmost importance. The Deutsche Gesetzliche Unfallversicherung (German Social Accident Insurance – DGUV) recognises this term to mean “medical, organisational and supportive measures for individuals who are ill or injured by means of simple measures including the involvement of the emergency services”.
Hierfür ist einerseits in Erster Hilfe geschultes Personal notwendig, das im Notfall eingreifen und dem Verletzten angemessen helfen kann. Andererseits muss der Betrieb dafür Sorge tragen, dass entsprechendes Hilfsmaterial zur Verfügung steht.
-
This includes items such as:
- Dressing material
- First aid boxes and cupboards
- Eye washing
- Dressing material
- Dressing material
- First aid boxes and cupboards
- Eye washing
Depending on type and size of the business as well as the occupational risks present, one or multiple first aid kits with different contents may be required. A manufacturing or processing workspace with 21 to 100 workers, for example, requires one (1) occupational first aid kit with a large capacity, in accordance with DIN 13169.
Additionally, employers must fit signs within their business so that first aid facilities, storage locations for dressing material as well as first aid areas can be located quickly.