Hoffmann Group
  • EN
  • DE
Skip to content
Hoffmann Group
  • PSA BEI DER HOFFMANN
  • AUGENSCHUTZ
  • ATEMSCHUTZ
  • HANDSCHUTZ
  • FUSSSCHUTZ
  • KOPF-UND GESICHTSSCHUTZ
  • GEHÖRSCHUTZ
  • SCHUTZ – UND ARBEITSKLEIDUNG
  • ABSTURZSICHERUNG
  • HAUTSCHUTZ UND ERSTE HILFE

FIND THE RIGHT SAFETY CLASS

Post navigation

Checking and maintaining fall protection
QUALITIES OF WORK AND SAFETY SHOES

Search

Recent Comments

    Archives

    Categories

    • No categories

    Meta

    • Log in
    • Entries feed
    • Comments feed
    • WordPress.org
    • EN
    • DE
    • PPE AT THE HOFFMANN GROUP
      Find out about the selection criteria that will help you choose the most suitable PPE.
    • EYE PROTECTION
      The right glasses for protecting your sight against damage.
    • RESPIRATORY
      PROTECTION
      Important selection criteria for the appropriate respirator.
    • HAND PROTECTION
      What matters when it comes to hand protection and how to create your own glove plan.
    • FOOT PROTECTION
      How injuries can be prevented with optimal foot protection.
    • HEAD AND
      FACE PROTECTION
      The right choice for working safely in all dangerous areas.
    • HEARING PROTECTION
      Maximum protection is achieved through hazard analysis, the selection of suitable products and wearing tests.
    • PROTECTIVE CLOTHING
      AND WORKWEAR
      Best protection for working safely in hazardous environments.
    • FALL PROTECTION
      Fall protection: Vital protection against deadly hazards.
    • SKIN PROTECTION
      AND FIRST AID
      Your tailor-made skin protection plan is only a few steps away.
    © 2026 Hoffmann Group | en

    | Imprint | Data Protection

    // Hearing protection

    Disposable earplugs

    Earplugs are basically inserted into the auditory canal and are especially well-suited to moist and warm environments. They also have good attenuation levels due to filtration of the noise levels, even at low frequencies.

    E-SHOP

    // Hearing protection

    Disposable earplugs

    This is how to insert disposable earplugs correctly:
    1. Roll the plug up as small as possible, ensuring it is crease-free. Make sure your hands are clean.

    2. Reach over your head with your free hand and pull the ear upwards and backwards. Insert the plug deeply into the auditory canal.

    3.& 4. Hold the plug firmly for approx. 30–40 seconds until it has fully expanded within the auditory canal. The earplug is correctly fitted in the ear if nothing is visible when viewed from the front.

    This is the correct way to remove and dispose of earplugs:
    When removing the earplug, pull it slowly out of the auditory canal with a slight twisting action. After use, disposable earplugs should be disposed of in the correct manner.

    // Hearing protection

    Disposable earplugs

    // Hearing protection

    Reusable earplugs

    Reusable earplugs can be reused without losing their original shape thanks to the washable surface. When you leave a noisy area, the earplugs can be put away in a handy storage box

    // Hearing protection

    Disposable earplugs

    This is how to wear earplugs correctly:

    1. Use one hand to grip the earplug by the stem. With the other hand pull the ear upwards and backwards whilst inserting the earplug into the auditory canal. Moving the ear up and down during insertion increases the protective effect.

    2. Even when correctly fitted, the plug remains visible from the outside.

    // Hearing protection

    Reusable earplugs

    In this short video, you can see how to wear ear defenders correctly.

     

    // Hearing protection

    Banded earplugs

    Banded earplugs are easy to use, comfortable to wear and can be put on and taken off quickly. The earplug does not sit in the auditory canal, instead it closes off the outer opening of the canal, which makes it pleasant to wear. It is suitable for working environments with high temperatures, since no heat build-up occurs. The earplugs can be replaced and the band can be reused

    E-SHOP

    // Hearing protection

    Banded earplugs

    This is how to wear banded earplugs correctly: 1. Grip the band under the chin with both hands. 2. Pulling the ear upwards and downwards whilst inserting the earplug increases the attenuation performance. 3. To check the fit, in a noisy environment press both earplugs slightly inwards. This should not make any great difference to the noise. Please note: 4. Pull the dirty earplug off the band. 5. Insert the new earplugs on to the band with a slight twist.

    E-SHOP

    // Hearing protection

    Banded earplugs

    In this short video, you will see how to wear banded earplugs correctly.

    E-SHOP

    // Hearing protection

    Electronic ear protection

    Hearing protection with special functions enables communication and simultaneous protection in the event of high noise levels. The noise-level-dependent attenuation technology means that warnings and instructions can audibly be received. Harmful noise is damped to a level less than 82 dB in order to protect hearing Additional functions: • Volume control of level-dependent function • Balance control • Equalizer ear defenders

    E-SHOP

    // Respiratory protection

    Particle masks

    Particulate respirators provide protection against particles. They are available as disposable masks in the following versions:

    1. Foldable: Practical for carrying around due to the flat, foldable mask body
    2. Pre-formed: Easy to use due to pre-formed mask body

    These protective masks are used during the grinding or sanding of brickwork, iron or paint as well as during the processing of glass and mineral fibres or asbestos, for example.

    E-SHOP

    // Respiratory protection

    Particle masks

    This is how you put the particulate respirator on properly:

    E-SHOP

    // Hearing protection

    Shell type ear protectors

    Ear defenders are particularly suitable for use in dirty environments and in environments where the noise level is continually changing. The shell envelopes the entire ear and the headband provides a stable and comfortable fit.

    E-SHOP

    // Hearing protection

    Shell type ear protectors

    This is how to wear ear defenders correctly: 1. For fold-away ear defenders fold the shells from inwards to outwards. 2. Place the shells over your ears. 3. Adjust the position of the band upwards and downwards. Please note: 4. To ensure the seal is tight, hair and the temples of glasses should not lie between the ear defender and the ear. 5. Die Ohren dürfen nicht mehr zu sehen sein.

    E-SHOP

    // Hearing protection

    Shell type ear protectors

    In combination with a safety helmet: 1.The ear defenders can easily be put on or taken off by clicking on and off. 2. When the ear defenders are not in use they can easily be swung away upwards.

    E-SHOP

    // Hearing protection

    Shell type ear protectors

    In this short video, you can see how to wear ear defenders correctly.

    E-SHOP

    Respiratory protection

    Full masks

    In order to protect yourself against gases and vapours, you need special gas masks. These re-usable masks are used in the event of frequent use and for wearing for long periods of time. These are also available as full-face masks, which also have a face cover.

    If the half-face and full-face masks are additionally required to provide protection against particles, then combination filters are the right choice. Here, particle and gas filters are integrated into a filter housing whereby the particle filter is always spatially arranged in front of the gas filter.

    E-shop

    Respiratory protection

    Half masks

    Here, you can find half-face masks, which offer a stable mask body that covers the mouth and nose: In order to protect yourself against gases and vapours, you need special gas masks. These re-usable masks are used in the event of frequent use and for wearing for long periods of time. For a start, here you can find half-face masks, which offer a stable mask body that covers the mouth and nose.

    E-shop

    Respiratory protection

    Respirator with blower unit systems / supplied air respirator systems

    Powered air purifying and supplied air systems are available for tough work environments and when equipment is worn for long periods:


    1. "Powered air purifying respirator systems:
      Filtration of ambient air without hindering breathing (O2 content > 17%)
    2. Supplied air respirator systems:
      Clean supply of air in the event of oxygen deficiency (O2 content ≤ 17%)"

    The powered air purifying respirator system is also available with a combination filter.

    E-shop

    Skin protection

    Moisturising skin care

    Skin should be cleaned before, during and after work. Products from this category gently remove dirt without unnecessarily irritating the skin. Their effectiveness depends on the product; from light to medium dirt up to extreme dirt, as well as strongly adhesive materials.

    E-shop

    Skin protection

    Important ingredients in skin protection products

    Similar to many skin care products, specific active ingredients support skin moisturising, reduce itchiness and promote healing:

    • Allantoin is a natural substance which promotes the healing of wounds and has cell-rejuvenating effects. It is used for alleviating skin irritations
    • Glycerine prevents the loss of moisture in the skin.
    • Witch hazel is a plant extract from the Hamamelidaceae family. It relieves slight itching and promotes the healing of wounds.
    • Panthenol is a provitamin. It strengthens the skin’s barrier function, increases the keratin layer’s ability to retain water, and improves the skin’s elasticity. Additionally, it reduces inflammation and itching.
    • Emulsifiers are another important ingredient within skin protection. They help to combine liquids that do not mix, such as water and oil, into an emulsion

    E-shop

    Skin protection

    Gentle skin cleansing

    Skin should be cleaned before, during and after work. Products from this category gently remove dirt without unnecessarily irritating the skin. Their effectiveness depends on the product; from light to medium dirt up to extreme dirt, as well as strongly adhesive materials.

    E-shop

    Skin protection

    Hygienic hand disinfection

    In occupational areas in which hygiene plays an important role, hand disinfection is vital. It prevents the transfer of germs, bacteria as well as viruses and should take place before, during and after work.

    E-shop

    Skin protection

    Accessories

    We hold a wide stock of products for skin protection, skin cleansing and skin care, together with the dispenser systems for their use, so we can offer you all you need to configure a clean and hygienic washing area.

    E-shop

    Fall prevention

    Safety harnesses

    Safety harnesses consist of straps fastened around the body. These catch the person as they fall, transmit the resulting forces on to appropriate parts of the body and keep the body upright.

    E-shop

    Fall prevention

    Attachment devices

    Attachment devices come in two basic designs: with a fixed and a moveable guide. On the fixed guide, the attachment device that moves with the user automatically locks and catches the user with the safety harness if they fall. The fixed guide restricts lateral movement. The attachment device with a moveable guide moves up and down the guide as the wearer moves. If the wearer falls, it locks automatically.

    E-shop

    Fall prevention

    Height security harnesses

    Height safety devices automatically catch and brake persons if they fall. They permit free movement within the cable extension range.

    E-shop

    Fall prevention

    Connectors

    Cables or straps with end connections are designated as connectors. Connecting elements connect the individual parts with a capture system. Fall dampers reduce impact forces acting on the person, the safety harness and the anchor device in the event of a fall.

    E-shop

    Fall prevention

    Anchor devices

    Anchor devices are made of different parts with one or more attachment points. These create a fixed connection between the system and the building or structure.

    E-shop

    Fall prevention

    Tool protection

    Fall prevention safety harness sets include all the parts which are required for basic equipment. These allow your employees to work safely on lifting platforms or roofs, for example. Additionally, the tools which your employees working at height are using should be prevented from falling so that people at ground level are not injured by falling objects. Special tool fall protection is available for this.

    E-shop

    Protective and work clothing

    T-Shirts

    E-shop

    Foot protection

    Safety low shoes

    Safety shoes can be worn all year round, are comfortable to walk or stand in, and also protect your feet at work. They are “classics” when it comes to foot protection. They ultimately cover the entire range of protective requirements, and in turn, are approved in many different companies.

    E-shop

    Foot protection

    Safety sandals

    Safety sandals stand out because they are highly breathable. This makes them especially well-suited to working indoors and in high temperatures outdoors.

    E-shop

    Foot protection

    Welder’s boots

    Whether in industry, manufacturing trades or production, wearing special safety shoes is prescribed for almost all metalworking jobs by the applicable Berufsgenossenschaft (employers' liability insurance association). These are work shoes that must meet certain standards to protect the feet from injuries and danger when working.

    E-shop

    Foot protection

    Business safety shoes

    For many people in management positions, a quick trip to the production hall or logistics area is a crucial component of day-to-day working life. A carefully assembled wardrobe including safety shoes should of course be a part of this. Our range includes a wide selection of business safety shoes which meet all the legal requirements, and also ensure a stylish appearance in every area.

    E-shop

    Foot protection

    Work shoes

    Good work shoes are ergonomic. They have an insole with a footbed that relieves the feet when walking or standing. They fit the foot firmly, without pressing on it. This reduces the risk of occupational illness. Work shoes are the ideal footwear for working in areas without mechanical risks.

    E-shop

    Foot protection

    Safety boots

    Boots of different protection classes with corresponding safety qualities are recommended, depending on the area of application. Boots of different protection classes with corresponding safety qualities are recommended, depending on the area of application. Alongside providing protection, it is also important that they are comfortable to wear.

    E-shop

    Eye protection

    SAFETY GLASSES WITH SIDE ARMS

    Safety glasses with side arms protect against mechanical hazards, such as during precision mechanical work.

    E-shop

    Eye protection

    SAFETY GOGGLES

    Safety goggles protect against eye injuries of both a physical and chemical nature, such as during dusty work like grinding or laboratory work.

    E-shop

    Eye protection

    WELDER’S GOGGLES

    A dazzlingly bright light with strong UV radiation is produced during electrical welding work. Without adequate protection, there is a risk of burns to the conjunctiva and irreversible injury. Furthermore, depending on the welding technique, harmful substances can be released which can also get inside the eyes.

    For this reason, welder’s goggles must meet strict requirements for eye protection. They must repel glare while ensuring excellent vision, protecting against UV light, offering scratch resistance and employing a suitable material to prevent burn-in of welding sparks.

    E-shop

    Hand protection

    MULTI-PURPOSE GLOVES

    Multi-purpose gloves are characterised by their suitability for a wide range of applications in day-to-day work.

    E-shop

    Hand protection

    LEATHER GLOVES

    In many manufacturing trades, leather gloves are the first choice for protective gloves that provide a high level of comfort for the wearer. Being a robust material, leather is not only resilient, but also soft and supple. These work glove qualities enable precise work, even when it comes to assembling small parts where sensitivity is required. Furthermore, leather gloves are suited to working in both cold environments and very hot ones.

    E-shop

    Hand protection

    CHEMICAL PROTECTIVE GLOVES

    Anybody whose job involves handling chemicals must take special precautionary measures. Dangerous gases or vapours are ingested through the nose and mouth 60 per cent of the time. This means suitable respiratory protection is required. However, up to 30 per cent of chemicals enter the human organism through the skin or mucous membranes and can cause irreversible damage.

    E-shop

    Hand protection

    ELECTRICIAN’S GLOVES

    Electrician’s gloves are special protective gloves that are furnished with an insulation layer to provide reliable protection against electric voltage. These can also be combined with an overglove, depending on the work application. This is especially important, as the effects of electricity on the body can cause significant harm, depending on the electrical resistance.

    E-shop

    // Head and face protection

    Safety helmets

    Helmets come in three different shell shapes: straight (1), straight with rain gutter (2)and with pulled-down neck and rain gutter (3). The industrial safety helmets are made of thermoplastic or thermoset, each with their own different properties and fields of use in construction, industry, hot operations and electrical engineering. More detailed information on this can be found on the label inside the helmet, for example. Special versions in this category are climbing helmets and forestry helmets.

    E-SHOP

    // Head and face protection

    Safety helmets

    Material types of industrial safety helmets:

    E-SHOP

    // Head and face protection

    Safety helmets

    E-SHOP

    // Head and face protection

    FACE PROTECTION

    Face protection is especially important if quickly flying particles, metal splashes, chemicals or electric arcs occur during work It consists of a protective visor which can be attached directly to a helmet or a head attachment.

    E-SHOP

    Head and face protection

    Impact caps

    In terms of their shape, bump caps are based on baseball caps. Due to their plastic insert, they offer light head protection, such as against stationary sharp-edged objects. They must not be used as a substitute for industrial safety helmets.

    E-shop

    Eye protection

    Prescription safety glasses

    Safety glasses with an integrated reading area enable precise detailed work.

    E-shop

    // Head and face protection

    WELDER'S MASKS

    Welding poses hazards, which include very high temperatures, against which employees must protect themselves. A welder’s mask protects the entire head and the face against radiation, heat and sparks. An integrated window with welding filter allows the employee to see his/her workstation. The highly modern automatic welder’s masks also boast several shade levels, which facilitate different kinds of welding work. Caps or hoods made from flame-retardant cotton can be worn underneath the mask.

    E-SHOP

    // Head and face protection

    WELDER'S MASKS

    E-SHOP

    Hand protection

    WELDER’S GLOVES

    High temperatures and radiated heat arise during welding work. Special welder’s gloves are required to adequately protect the hands. They are considerably longer than other work gloves in order to offer the wrist and the lower arm protection as well. These gloves can also be combined with welder’s hand protection, which provides extra protection against heat and radiated heat.

    E-shop

    Hand protection

    CUT-RESISTANT GLOVES

    Cut-resistant gloves enable the user to avoid injuries due to cuts from sharp-edged tools and working materials. Whether in assembly, metalworking or glass working, in the food or automotive industry, cut-resistant gloves significantly reduce the risk of injuries to the hands from cuts, without limiting the freedom of movement at work. overview of cut protection

    E-shop