| There are a large number of criteria that must be taken into consideration when choosing the best-suited work gloves.
The field of application is of particular importance. Is the environment dry, or is it more of a damp and oily workplace? Do the gloves need to allow sensitivity and precision for the relevant activity, or do they need to help with heavy-duty work? Which hazards do the gloves need to protect against? In order to fulfil these varied demands, work gloves are made from a wide range of materials. Wearing comfort also plays an important role in choosing the gloves. |